1. Knowledge Base
  2. Palletizing Solution

Ignore collision between gripper and box at trajectory start

When using the find surface to put the box on the pallet, the gripper can be in a theoretical collision model. Therefore, a collision detected pop-up appears.

 

Before using the presented function check the pallet height and the box height before.

 

If the problem persists this is the situation to use this function.

 

Description : 

Determines if a detected collision
between the boxes and the gripper is allowed when leaving the Release folder (used when a Find Surface or
a similar method is used to gently place the box lower than expected).

 

How ? 

To access advanced feature like collision model, you need to add a feature point named: RQ_PAL_JSON and teach this point.

 

Where to add ?

Then you will have access to the additional JSON parameter Field

What to add ?

[JSON] allowCollisionsBetweenGripperAndBoxesOnPalletAtTrajectoryStart

Description

Ignore collision at the beginning of trajectory after exiting release folder. Best when using a Find surface at the release like in depalletizing or when the boxes have variable heights.

Declaration

{"allowCollisionsBetweenGripperAndBoxesOnPalletAtTrajectoryStart": isAllowed}

Parameters

isAllowed (type: bool)

Example

{"allowCollisionsBetweenGripperAndBoxesOnPalletAtTrajectoryStart": True}