Controlling a Robotiq Gripper on a UR CB2
Use the legacy driver package to operate your 2F-85, 2F-140, or Hand-E gripper on older UR controllers
UR CB2 controllers do not support URCaps, which are required for Robotiq's gripper integration. However, you can still control your Robotiq gripper (2F-85, 2F-140, Hand-E) using a legacy driver package available in our support archives.
1. CB2 Controller Limitations
URCaps were introduced with CB3 and later versions. CB2 controllers do not support this feature.
This means you cannot use the newer, more user-friendly Robotiq URCap packages with CB2 systems.
2. Recommended Solution: Use the Legacy Driver Package
Robotiq provides a legacy "Driver Package" that includes the Gripper Toolbar.
This package enables basic control of the gripper on CB2 controllers.
You can find it in the Archives section of our support site.
3. Compatibility Reference
Refer to the table below to see which Robotiq software packages work with each UR controller type:
4. Setup Notes
The legacy driver is less intuitive than URCaps but effective for basic use.
Follow the instructions included in the archive to install and configure the driver on your robot.
Conclusion
While CB2 controllers are not compatible with modern URCaps, Robotiq's legacy driver package provides a practical workaround.
Need help? Contact Robotiq Support.
Updated: August 13, 2026