Make sure to keep track of defects so you can work on the problems that have the most impact on your production; those are not necessarily the problems that are the most visible.
So if you are changing suppliers or some components, make sure that the new ones are just as good as the ones you had before. Also be careful when putting pressure on manual labor to produce more. This may create some tensions within the company and actually lead to lower productivity rather than faster production. The other aspect to quality control and productivity is that to perform quality control along the production chain takes time.
Going overboard on quality is just as bad as not doing enough: you’re not adding value to your production. You may need to scrap some products for quality testing or you may have some employees working full time just on quality control. The good news is that by automating some tasks you should get better quality control, because if there is one thing everyone can agree on, it is that robots are good at doing repetitive tasks. So there will be no need to spend as much time inspecting for quality.
Furthermore, because of the repeatability of the robotic process, the chances of some parts failing between batch testing is reduced. Also there might be some data that would be accessible through the robot that would allow you to flag potential errors, like a glue level alarm or a low glue flow alarm and so on. You can probably also flag when a quality test needs to be done after a certain number of cycles performed by the robot. This way you can test both for the quality of the glue and the accuracy of the robot.
Read more about optimizing productivity in our eBook: Optimizing the Productivity of Existing Equipment.