In our last edition of the Ebook, the German manufacturer KUKA was not on the list, however, we were informed that one of their collaborator's designed a technology package that allows for safe human interaction.
The company MRK-Systeme GmbH provides automation solutions for many industrial sectors. They are specialized in safety systems that allow human-robot collaboration. So they are presenting the 'Kleinroboter' or small robot, KR 5 SI (for Safe Interaction).
This is a technology package that is an option for the KR 5 ARC HW KUKA’s low payload robot. This option is able to transform ordinary industrial robots into a collaborative robot approved by DIN EN ISO 10218 and TS 15066 regulations. The certification system is one reason why physical separation is no longer needed between robots and humans.
The system is based on 5 functionalities:
With all these components, the robot is classified as safe for human interaction. However, it is important to mention that working around a robot, in general, will always have some risks and a worker should always be aware of that and work wisely around any industrial robot.
This system can be used in at least two applications: a carrying measurement system and material handling.
As an example for the measurement system, the robot could hold a camera in order to do automated inspections. (Quality Insurance)
Or, for a material handling application, the robot could be used in a machine loading and unloading task. (Pick-and-Place)
For more information on this new collaborative robot, see the company website: MRK-SYSTEME GMBH