When your product is frosting and your goal is to move it—fast, clean, and without breaking a sweat—you don’t want to leave anything to chance. That’s exactly why one bakery manufacturer teamed up with Robotiq and Alba to automate their bucket palletizing process. The mission? Stack a variety of frosting bucket sizes onto CHEP and GMA pallets without manual labor or downtime.
Spoiler alert: mission accomplished.
The bakery needed a better way to palletize heavy buckets of frosting. The old-school method—manually stacking both sides of the pallet—was inefficient and tough on workers. To make matters more complicated, they didn’t want to dedicate staff just to place empty pallets on the conveyor.
So, we brought in the heavy hitters:
The result? A fully automated setup that palletizes 57 lb loads with precision—and zero strain on the workforce.
The real magic was in the integration. Alba supplied a pallet dispenser that automatically delivered empty pallets to the build zone. From there, the AX30, enhanced with a seventh Z-axis, tackled palletizing with the reach and flexibility the application demanded.
To support the cobot’s movements, Alba designed a conveyor system that did more than move product—it made the entire process smarter:
With this system in place, the line ran autonomously—requiring just a forklift driver to remove full pallets. Talk about efficient teamwork.
With repeatability baked in and heavy lifting handled by the cobot, the system now delivers up to 15 full pallets per hour. That's 2,736 lbs of frosting goodness per pallet, effortlessly moved and stacked, while operators focus on higher-value tasks.
They also added:
At Robotiq, we follow the Lean Robotics methodology—Design → Integrate → Operate—to keep automation simple, scalable, and smart. This project checked every box:
✅ Labor reallocation
✅ Improved ergonomics
✅ Flexible solution for different bucket sizes
✅ Fast deployment
✅ Smooth integration with Alba’s conveyor tech
It’s a textbook example of how collaboration turns challenges into sweet victories.
Got repetitive tasks eating up your team’s time?
Let’s build something better, together.
➡️ Talk with a Robotiq expert and start designing your next smart automation move.