Subscribe

Latest Blog Post

part presentation playbook

Top 3 reasons to automate your small-medium enterprise

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette on Nov 10, 2015 3:30:00 PM

As a small-medium enterprise you probably ask yourself how you could increase your margin, increasing your production and reduce your cost? Well, this is the struggle of everybody in this size enterprise. Most of the time, you will have a product that is unique or which will add value to another major manufacturer. However, to make your way in the market; you need to increase your production, reduce your cost and enhance your product quality. Well, a part of the solution might be robots.

In fact, most of the SME's we have visited have all been stuck with the same problems: workforce is hard to find, production is going to fast for the number of workers, so quality is suffering. Well, introducing a collaborative robot like Universal Robots into your manufacturing process can help you solve these problems. 

 

 

** The video features a Universal Robots UR5 and a Robotiq 2-Finger 140 Adaptive Gripper **

In fact, here are 3 reasons why you should automate your manufacturing process with a collaborative robot. 

1. Saving $$$

Collaborative robots have a very fast return on investment (ROI). In fact, most of the people who will introduce a collaborative robot into their production line will refund it in less than 6 months. So as you are struggling with workforce problems a robot can be a cheap option to cover the lack of people. It can be placed in almost any working post that requires dexterity or repetitive tasks. You can then leave the robot run on its own and let your employee add value to the product by doing setups and quality inspections instead of standing in front of the machine all day. 

2. Quality +++ 

A product’s quality reflects the reputation of the company. If you are delivering poor quality product, your customers will certainly hesitate to buy your product again. On the other side, if you deliver good quality product, you will be able to build a strong network of customers and they will refer others to you. You can achieve this quality by having a constant process. If the robot is tending a machine or pick-and-placing parts on a conveyor, this is time that can be repurposed for quality checks.  

universal-robot-robotiq-gripper** A collaborative robot doing product testing on a batch of electronic components** 

3. Production +++

Reducing time spent in front of the machine means time to prepare the next changeover. This also means your machine will be stopped a minimal amount of time and you will be back in production in the blink of an eye. You will then be increasing your production rate without any major changes to your enterprise. 

Notice that some manufacturers will use several robots on rolling stations, so they can move them around the plant. Because of the ease of programming for collaborative robots, it is sometimes even easier to re-teach points than to find the program for the next job. 

You must be asking yourself ? “What’s the price of this incredible solution?'' Well, remain calm. Here it goes. 

Universal Robots depending of the model will be around $35,000 USD. A tool like the Robotiq's 2-Finger 85 Adaptive Gripper will be around $5,000 USD, then you will need to add a couple of fixtures and other components to your cell to adapt it to your application for an average total of around $50,000 USD. Notice that no additional safety devices are required to install with a collaborative robot. These robots are safe to work around humans under certain conditions and, of course, a risk assessment is must be properly completed. 

With cobots you enhance your product quality, your production is a lot faster and a lot of employees stop doing redundant (and exhausting) tasks, while your return on investment is quite fast. This is why at this price it's not long before you are looking for other places to install your next robot. 

Related Articles:

Collaborative robots change SME productivity

Compare 19 collaborative robots
Get the chart here

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mathieu Bélanger-Barrette
Mathieu works as the production engineer at Robotiq, where he strives to constantly optimize the production line for Robotiq Grippers. Mathieu is always looking for new manufacturing processes to make operators as efficient as possible. He is also seeking out new robotic applications and their effect on improving our world, then keeps Robotiq’s blog readers updated on his finds.
Connect with the writer:

Related posts

Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016
Trending on DoF This Week - Nov. 10

What's trending on DoF this week? Screw insertion using Robotiq camera, Robotiq products weights, bottle packaging with UR and...

Amanda Lee
By Amanda Lee - November 10, 2016

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more