Subscribe

Latest Blog Post

New Call-to-action

Robotiq Gripper Helps to Produce Other Grippers

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette on Aug 25, 2016 7:00:00 AM

We recently went to one of our vendors to see its latest robotic cell. Précinov based in Lévis, Canada introduced a robotic cell a couple of months ago and can already see the benefits from it. We made a short interview with Mathieu Deblois, founder of the company. 

IMG_3341.jpg


Robotiq Products

Since Précinov is manufacturing some of the parts that are used in our Robotiq products, they were certainly curious to use the entire solution and see its benefits. We went there to see what was his impression and without even asking for it, he literally told us what we wanted to hear! No kidding. Mathieu was really impressed by the versatility of the Gripper and he tried to design his robotic cell to fit with the flexibility of the Gripper. 

''This is not an installation designed to make one part type in a week or a month. It is really designed for one part type per day or even during an evening, we can make up to four different types of parts.''

The robotic cell is fed by a conveyor with 4 different alleys. Each of these alleys have proximity sensors that detect the presence of a part, but also trigger which program should be run in the machine for this precise blank part. Depending on the production, you can run the 4 alleys with the same program or with up to 4 different part models. This allows Précinov to produce a lot of different parts at a fast rate and without worrying about loading and unloading the machine. 

''With the same Gripper we can take parts of different sizes. I would even argue that the problem is not the Gripper but the vise in the machine that does not have the same flexibility.''

With such installations, the machine shop has seen its productivity increased by 20% only by letting the machine run during the night and weekends. This is only one of the benefits that a machine tending cell can bring to a company.

Stay tuned for our other articles on part 2 and 3 of our interview with Mathieu about the integration and the reaction of employees towards having a robot on their work floor.

New Call-to-action 

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mathieu Bélanger-Barrette
Mathieu works as the production engineer at Robotiq, where he strives to constantly optimize the production line for Robotiq Grippers. Mathieu is always looking for new manufacturing processes to make operators as efficient as possible. He is also seeking out new robotic applications and their effect on improving our world, then keeps Robotiq’s blog readers updated on his finds.
Connect with the writer:

Related posts

Accelerate Your Robot Programming With This New Template

What's trending on DoF this week? Measuring insertion force, Robotiq 2-Finger 85 Gripper on Kuka IIWA, reset controller after...

Amanda Lee
By Amanda Lee - April 27, 2017
How Easy it Is to Introduce a Robot: A Case Study

Introducing a robot can sometimes be scary for somebody who has never done it. However, there is a way to make it easy for you...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - October 4, 2016

How to troubleshoot images with Robotiq camera

Hi pros,how do you guys troubleshoot images with the Robotiq camera. In one of our application we have a snapshop position during production that is different than the snapshot position that we have...Read more

Problem with camera software upgrade

Hello all, I'm having trouble after I updated to the newest version of the camera update. I'm using a UR3, updated from UCC-1.2.0 to UCC-1.2.1. Here is the problem: - The centering part...Read more

Universal Robots controller upgrade kit to 3.1

Hi everyone, we had a bunch of questions and request concerning the Robotiq product compatibility over UR. Remember that the Camera is compatible for UR with controller 3.1 only while our other...Read more

Robotiq grippers on robot arm

Hello,I am a ROS user and I'm working with a robotiq gripper attached to an sia5 motoman arm. It looks like this:http://www.youtube.com/watch?v=TwXBoyqP__U&feature=youtu.beI've got the arm...Read more