Subscribe

Latest Blog Post

compare new collaborative robots

PODCAST Episode Three: Gurvinder singh Virk

Emmet Cole
by Emmet Cole on Dec 3, 2015 7:00:00 AM

Our guest in this edition of Robotiq's podcast series is Gurvinder Singh Virk, a professor of robotics at the University of Gävle in Sweden and an expert in robot safety standards.  

Gurvinder Singh Virk is chairman of the International Standardization Organization group that developed ISO 13482 --the world's first ISO standard for personal care robots, released in early 2014.  

"Robots and humans are definitely going to be co-sharing the space. I think the whole community really wants this to happen. It has to be done in a coherent way. The only way we can achieve that is for the international community to work together to define those rules and how those requirements and rules should be rolled out. [This] needs to be done holistically. It can't be done piecemeal by one region or one country." stated Mr. Virk.

Listen to our interview to hear Virk's insights on a range of topics, including: iso_logo.gif

  • What exactly are robot standards
  • Why they are important for the growth of the industry 
  • Which region is leading the way in the adoption of ISO 13482 (and which regions are lagging behind) 
  • The special safety challenges presented by cobots in industrial settings 
  • The key principles behind any safe, collaborative human-robot installation 
  • ...and more.

Did you know that Robotiq's CTO, Jean-Philippe Jobin, is involved in the development of ISO/DTS 15066? Find out more here at the ISO webpage.

 

LISTEN TO THE PODCAST NOW

 

 
x

Subscribe to Robotiq's Blog

Leave a comment

Emmet Cole
Written by Emmet Cole
A freelance robotics writer since 2006, Emmet is an Economist contributor, and a regular contributor to Robotics Business Review and Robotics Trends. His writing on robots has also appeared in Wired, BBC Future, BBC Focus magazine, Space Quarterly, and numerous other outlets.
Connect with the writer:

Related posts

PODCAST: Heni Ben Amor

Assistant professor, Heni Ben Amor, uses the Robotiq 3-Finger Adaptive Gripper for human-robot collaboration. Aim... to develop...

Emmet Cole
By Emmet Cole - October 2, 2015
Robotiq at IROS 2011

Robotiq will exhibit at the 2011 International Conference on Intelligent Robots and Systems (IROS) being held in San Francisco...

Samuel Bouchard
By Samuel Bouchard - September 16, 2011

2 Finger Gripper(85) on a Universal Robot 5

I need to have in ROS Gazebo and MoveIt an UR5 robot who has the Robotiq 2 Finger Gripper(85) in the simulation models. At the moment all I have is the UR5 model only for simulations. How do I add...Read more

open source robot arm

Hi everyone,  how can I get a low cost open source robot arm for my final year projet.Thanks.PRINCEWILL Read more

How to integrate robotiq arm with motoman SDA10F moveit config

Hello,I was reading and following what @carlosjoserg posted here, but I get the following error when integrating my robot xacro with the gripper xacro.I attach the picture of my file and the...Read more

wrist camera

i have UR10 universal robot to pick small round  plastic part (28 mm in diameter& 18mm high ) which has rectangler slot in centre of it and gets fed by vibration bowl feeder to the same...Read more