Subscribe

Latest Blog Post

build your in-house robotic expertise program

Start Picking Your Objects Efficiently With the Wrist Camera and 2-Finger Gripper

Amanda Lee
by Amanda Lee on Aug 10, 2017 7:00:00 AM

What's happening on DoF this week? New program template helps you save time by picking parts without any waypoints or Gripper moves. Help the Pros by calculating geometric models of a mobile manipulator and placing sub-programs efficiently. Learn more from automation Pros here!

Easily Auto-Pick Your Objects With the Wrist Camera and 2-Finger Gripper

A new program template is now available on DoF to help you save time picking your parts with the Wrist Camera and the 2-Finger GripperIt contains a script function that allows the robot to automatically pick an object that has been previously taught to the vision system without having to teach waypoints and Gripper actions. Take a look at the final result below.


Calculate Geometric Models of a Mobile Manipulator

Samir a PhD student wants help with his thesis about developing a new control law for a mobile manipulator. So far he was able to determine the direct geometric model for the mobile manipulator (mobile Base + Manipulator) , but didn’t succeed in calculating the inverse geometric model of the mobile manipulator (Base+Manipulator). Do you know how to? If so, help him out!

Suggest Efficient Sub-Programs

Matthewd92 is always helping out other DoF members on the community! Recently it was the case for AZalmanov concerning the placement of his sub-programs. Matthew came up with a great example of code that Anthony can easily use in his program. Take a look into the solution! Or maybe you have an alternative to suggest?

 Did we miss anything?  Ask the Pros on DoF!

choose the right collaborative robot

 
x

Subscribe to Robotiq's Blog

Leave a comment

Amanda Lee
Written by Amanda Lee
As an e-marketing coordinator, Amanda focuses on Robotiq's content management. With her background in marketing, she hopes to bring valuable, relevant, and consistent content to our audience through the blog, social media and video center.
Connect with the writer:

Related posts

An All-Inclusive Collaborative Robot Solution at the Fraction of the Price

We have been seeing a lot of new collaborative robot companies appear in the last few years. Most of them (in opposite to...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - August 2, 2017
A Collaborative Robot Performing Several Assembly Steps

Creating Revolution is a Miami Startup producing a hospitality pager that connect the customer's smartphone to the waiter....

David Maltais
By David Maltais - July 12, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more