Robotic Task Mapping

Once your Manual Task Map is done, you are ready to figure out its robotic equivalent, the robotic task mapping. The thing about robotic task mapping is you can’t complete it without knowing the layout—but you also can’t complete the layout without knowing the task map! That’s why we suggest working on these two components together.

The Robotic Task Mapping Template takes the same structure as the manual map. Complete it to be ready to do the manual-robotic comparison. We’ve also included an example of a robotic task mapping to validate your own work.

Fill-in the form on the right to get the Robotic Task Mapping resources.

media-20170905 (1).png

Download Robotic Task Mapping Resources