Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

ISO/TS 15066 for the Real World: Product Assembly

Karine Simard
by Karine Simard. Last updated on Jun 10, 2016 10:46 AM
Posted on Jun 08, 2016 7:00 AM. 2 min read time

Picture a sequential product assembly process that includes both humans and power and force limited collaborative robots, suggests Björn Matthias, Senior Principal Scientist – Robotic Automation, at ABB.

_U4A2705_HD.jpg

Robots perform the simple steps where repeatability generates quality while human workers perform more complicated steps, particularly those that require highly dexterous manipulation.

When performing a risk assessment in a scenario like this, it's important to identify the interfaces between the human and robot workers.

“As it is being manufactured, the product passes over these interfaces. You have handover and you have assembly manipulation and these things are happening right next to human workers,” explains Matthias.

In this sample scenario, possible hazards occur at the interfaces; the area where workers reach into the robot's workspace for example. A different set of hazards arise when human workers accidentally bump into the robot.

“Mitigation of these hazards --and the way you can make the system harmless-- is by designing the robot's control system so that it enforces the maximum limits on mechanical loading of certain parts of the human body.”

If you follow the ISO/TS 15066 guidelines for power and force limited applications, which specify maximum pressures and maximum forces, you will be able to realize this type of sequential assembly landscape in a safe way and all without having to separate the robot off behind fixed guarding.

“That is the aspect which is very new in ISO/TS 15066.” adds Matthias. “This is also the aspect which addresses the need for higher flexibility and less use of floor space that today's manufacturers are looking for.”

 

How to Perform an ISO/TS 15066-Compliant Risk Assessment

How-to-perform-risk-assessment-ebook-cover-1.pngReady to get started with improved safety with collaborative robots? This is your guide.  This eBook explains each part of the document, how to fill it up, and why it's there. Follow the guide to perform those risk assessments and comply with ISO/TS 15066. This eBook also comes with an Excel template for you to use.

Get the eBook now!

 

Leave a comment

Karine Simard
Written by Karine Simard
Karine is a journalism-school graduate turned marketer with a side-step in sales and the addition of an MBA to complete her understanding of business. She has documented, marketed and sold products in the high-tech industry, from power monitors to people counters, enterprise software and telecom testing solutions. She cares about team dynamics, marketing and generating quality leads for her teammates in sales. Her mission is to bring sales and marketing teams together into one happy revenue-generating machine.
Connect with the writer:
http://robotiq.com

Related posts

15 Mistakes People Make With Cobot Safety

Even collaborative robots can have safety problems, but only if you make a mistake. Here are 15 common mistakes that people...

Alex Owen-Hill
By Alex Owen-Hill - November 6, 2018
How to Perform a Risk Assessment for Collaborative Robots

There's no doubt that collaborative robots have shaken up the industrial market, given their revolutionary ability to interact...

Mariane Davids
By Mariane Davids - May 7, 2018
Risk Assessment for the Robotiq 2-Finger Gripper

 Assessing the risks of a collaborative robot is a complex process. It involves many different risks, probabilities, and – most...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - April 19, 2018