Subscribe

Latest Blog Post

build your in-house robotic expertise program

Help Out the Pros With Their Robotic Integration Projects

Amanda Lee
by Amanda Lee on Jul 20, 2017 7:00:00 AM

What's happening on DoF this week? A Pro wants your help automating a sachet guiding process on a conveyor belt. A new program template is out enabling you to find, measure and locate the center of a part with the Force Torque Sensor. And don't forget to help Steven with his palletizing application. Learn more from automation Pros here!

Picking up Sachets From a Conveyor Belt With a Robot 

1mwdsl27xb6n-230653-edited.jpg

This week, abdeldayem5 wants to automate a process in his shop and needs your help! He explains that sachets come out randomly of a pasteurization tunnel on a conveyor. He then wants the robot to pick up these sachets from the conveyor belt and stack them into a box. 

Is using a vision system the solution as Matthewd92 suggested? Or maybe using a new chute system as proposed by Mhowe? Let us know what you think in this new DoF discussion!

New Program Template: Locate the Center of a Part With the Force Torque Sensor

 

Another useful program template is now available for you to download! This one is used with the Force Torque Sensor allowing you to perform search instructions in the X, Y or Z axis of the tool to locate parts. Also this program template gives you the capacity to measure an object by using the Find function on both sides of it. Take a look at the video above to see the capabilities of the Force Torque Sensor while using this program template and start using it in your program right away!

Help Steven With His Palletizing Application Project

palletizing.png

Another interesting robotic project was shared on the community this week by Ssandberg. He has a robot picking up parts from a table but the table occasionally moves a few inches. He wants to know if there is a way to change the pallet reference without the need to teach the various pallet points once again. Anything to suggest to Steven?

 Did we miss anything?  Ask the Pros on DoF!

solve the skills gap in manufacturing

 
x

Subscribe to Robotiq's Blog

Leave a comment

Amanda Lee
Written by Amanda Lee
As an e-marketing coordinator, Amanda focuses on Robotiq's content management. With her background in marketing, she hopes to bring valuable, relevant, and consistent content to our audience through the blog, social media and video center.
Connect with the writer:

Related posts

Are Your Robots Correctly Secured?

What's happening on DoF this week?

  • Secure your robots to make sure they don't get compromised!
  • New application package: Path...
Amanda Lee
By Amanda Lee - August 31, 2017
Help Out the Pros With Their Vision Systems

What's happening on DoF this week? Everything Wrist Camera!

  • Help out a Pro eliminate motion blur when using his vision system
  • ...
Amanda Lee
By Amanda Lee - August 24, 2017
Palletize Over 50 Different Pallet Layouts With a Universal Robot

What's happening on DoF this week?

  • Help out a Pro with his palletizing project using up to 50 different pallets.
  • Have you...
Amanda Lee
By Amanda Lee - August 17, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more