Subscribe

Latest Blog Post

build your in-house robotic expertise program

Getting Started with Collaborative Robots: Product Testing

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette on Mar 23, 2016 7:00:00 AM

You are looking at your first robot integration, you have heard about collaborative robots, but you don't know where to start? You’ve come to the right place. We have put together this blog post series to help you figure out which robot will match your specific application. For our third blog post, we'll talk about product testing applications. The first post on machine tending can be found here, and our second post on assembly applications is here

What is product testing?

Whatever you are doing as a manufacturer, you most likely have product testing and/or quality checkpoints where your product is tested. If a step is skipped or a part is wrong, this step of the manufacturing process will trigger an error and will tell you that your product is defective. As some tests have a long run cycle and employees have more interesting things to do than pushing on 27 different buttons in a given order, robots can be introduced to perform this task. 

What about product testing with a collaborative robot?

A collaborative robot or cobot for short, is a general term used to describe power and force limited robots. Robots that can be used without safety guarding or that incorporate other safety features. This means a cobot can be put beside a machine or a person and set to perform a certain task without needing to be fenced off from its surrounding environment.

That being said, to introduce a cobot on an assembly line or beside a test bench and program it to test parts is not as simple as it sounds. You will need to choose a robot that can accomplish the job and that can reach a level of performance comparable to a human worker. To help you, we have listed some key factors you might consider for product testing if you are using a collaborative robot. 

Robot Specs
repeatability_2_-_Copie.png

  • Repeatability: The robot has to be consistent in its motions to test products with tight tolerances. In fact, with small/fragile parts such as a printed circuit board (PCB), you need to be highly repeatable in order to test the products and make sure not to damage anything as a result of the testing process. You will need to choose a robot than can meet your application’s demands in terms of repeatability.
    Tip 1: If you need to repeat a given action an infinite number of times, make sure to buy a robot that can respect the position tolerance you need to achieve.
  • Speed: In some product testing applications, speed is very important. Granulated speed control can make a difference in your product testing, but it can also play a huge role in your cycle time.

Gripper Specs

force_feedback.png

  • Force Feedback: We see, daily, a lot of applications that require force feedback. Using a force torque sensor will allow you to have consistent force/pressure applied on a given region of the product for whatever you want to do. This means that you can limit the force at a given point and collect this information for your database.
    Tip 1: Make sure the force torque sensor used can carry the payload of your heaviest part.
  • Flexibility: As seen in the video above, you may need to carry different kinds of objects, as well as open or close doors to achieve your product testing. This means that a flexible gripper is probably necessary.
    Tip 1: Super flexible grippers (5 fingers for example) usually have a low payload and very high price point. Make sure you are using a gripper that meets your payload requirements and that is strong enough to perform your industrial application. 
    Tip 2: Go for an electric Gripper, they are easier to implement and reduce the integration time. 

Required Workspace

  • Safety: The robot will work alongside humans. Some will be aware of the dangers this presents, others won't. Make sure to perform a risk assessment before building your automation project. Once you're ready to go live, make sure everyone is trained on safety rules around the robot and the risks involved with using a robot. Collaborative robots are safe, but can still represent risks to the workers.
    Tip 1: Upictos_robotiq_Juin2015_VF-9_-_Copie.pngse ISO standards to guide your risk assessment and don't forget to consult local regulations on this subject. To learn more, download this eBook on risk assessments for collaborative robots
    Tip 2: Remember, even if the robot itself is safe, if the tool or the part it carries is dangerous, then the robot cell in and of itself poses risks for your workers. 
  • Machine Interface: Make sure to interface your robot with the machine you will be using. Most of the time a programmable logic controller (PLC) or a simple PC will be used to perform the testing or collect data. 
    Tip 1: This seems simple, but this is probably the most complex part of the process. Make sure to reserve time and budget for this one. 

 

There you have it, this is a basic overview of robot, gripper and workplace specifications that you might consider if you are thinking about implementing a cobot to do your product testing. If you need more information on how to shop for a collaborative robot or what key features of a cobot might be important according to your application, we have put together a complete eBook on this subject. Or you can contact one of our application engineers who would be happy to discuss your automation projects. 

GET THE EBOOK ON HOW TO SHOP FOR A COLLABORATIVE ROBOT

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mathieu Bélanger-Barrette
Mathieu works as the production engineer at Robotiq, where he strives to constantly optimize the production line for Robotiq Grippers. Mathieu is always looking for new manufacturing processes to make operators as efficient as possible. He is also seeking out new robotic applications and their effect on improving our world, then keeps Robotiq’s blog readers updated on his finds.
Connect with the writer:

Related posts

What's New in Robotics This Week - Apr 21

Industrial & cobot roundup, meet the cheetah bot, drone brief (land & air), a good time to mention ISO/TS 15066, and much more. 

Emmet Cole
By Emmet Cole - April 21, 2017
How Much Programming Skill Do You Need to Train Collaborative Robots?

Collaborative robots are bringing a new wave of innovation to countless industries in the field of manufacturing. They can work...

Mariane Davids
By Mariane Davids - April 19, 2017
Pallets + Robots = a Competitive Advantage?

Palletizing is a trending application for collaborative robots. Could it give a competitive edge to your business? We look at...

Alex Owen-Hill
By Alex Owen-Hill - April 18, 2017