COMPARE 59 INDUSTRIAL ROBOTS WITH A PAYLOAD OF BETWEEN 5-10KG

Are you looking to get a new industrial robot with a payload from 5 to 10 kg? We have gathered all the main specifications for more than 59 industrial robots from 14 robot manufacturers, namely: Yaskawa, Kuka, ABB, FANUC, Universal Robots, Staübli, Comau, Denso, Adept, Kawasaki, Mitsubishi, Nachi, Toshiba and Epson.

See in the blink of an eye robot specifications, such as:

  • Payload
  • Reach (vertical & horizontal)
  • Repeatability
  • IP Rating
  • Robot Mass
  • Hollow Wrist
  • Controller

FILL OUT THE FORM ON THE RIGHT SIDE OF THIS PAGE TO GET YOUR COMPARATIVE CHART!