COMPARE 44 INDUSTRIAL ROBOTS WITH PAYLOADS BETWEEN 20-50 KG

Are you looking for a new industrial robot with a payload from 20 to 50 kg? We have gathered all the main specifications for more than 40 industrial robots from 9 robot manufacturers, namely: Yaskawa, Kuka, ABB, FANUC, Staübli, Comau, Adept, and Kawasaki.

See in a flash the robot specifications, such as:

  • Payload
  • Reach (vertical & horizontal)
  • Repeatability
  • IP Rating
  • Robot Mass
  • Hollow Wrist
  • Controller

FILL OUT THE FORM ON THE RIGHT SIDE OF THIS PAGE TO GET YOUR COMPARATIVE CHART!