Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Risk Assessments for Collaborative Robots - Updated eBook

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette. Last updated on Mar 14, 2016 9:06 AM
Posted on Mar 14, 2016 9:00 AM. 2 min read time

Following the release of the ISO/TS 15066 and the popularity of our eBook on Collaborative Robot Risk Assessment; we thought it might be appreciated if we were to put them together. So, we have provided a colloquial view of the new technical specification and merged it into a new eBook. Since the tech spec is pretty dense and statistically oriented, it can be tough to understand. We have underlined the main features and tried to bring them to you in an insightful way in a convenient format. 

ISO/TS 15066 - SO WHAT?

_MG_2105_HD.jpg

Collaborative robots are being scrutinize to determine their compatibility with many different standards. The ISO/TS 15066 is only one of several regulations that may apply to ensure worker safety when using collaborative robots. Previously ISO 10218 was the primary standard that was used in guiding collaborative robot safety. However, ISO 10218 was not particularly well matched to the power and force limited cobots that are popular today. In 2011 when the standard was adopted there were very few collaborative robots or applications actually in place. Therefore it is welcoming news that some precision and guidelines are now available for manufacturers and integrators of collaborative robots. 

EBook Content

In this eBook we define a lot of different terms and provide common meanings. Since our goal is to help you integrate robots and free human hands from tedious tasks; we want you to use cobots as your coworkers. We want to get straight to the point with definitions that will help you figure out what is a risk assessment and how you can realize one. 

What's next?

So if you are a DIY kind of person or merely looking for more information on the risk assessment process, I think you will like this new updated risk assessment eBook for cobots. You can download the latest version by clicking this big colored button at the button of the page. 

 GET THE EBOOK ON COLLABORATIVE ROBOT RISK ASSESSMENT

 

Leave a comment

Mathieu Bélanger-Barrette
Mathieu is a production engineer at Robotiq, where he constantly strives to optimize the production line for Robotiq Grippers. He enjoys discovering new robotic applications and sharing what he learns on Robotiq's blog.
Connect with the writer:
http://robotiq.com

Related posts

8 Benefits of Palletizing Cobots in the Coffee and Tea Packaging Process

The coffee industry is very competitive. If you're looking for a way to solve labor shortages, speed up your processes, reduce...

Nicolas Lauzier
By Nicolas Lauzier - November 16, 2022
How to capture sharper images of moving objects

So you’d like to count or inspect moving objects?  Here are a few tips that might help you out.

You can work with a few...

Audrey Boucher-Genesse
By Audrey Boucher-Genesse - May 7, 2020
Surface Finishing: The Essential Guide for Busy People

Surface finishing makes the difference between a quality product and a bargain-bin reject. This guide explains how to choose...

Alex Owen-Hill
By Alex Owen-Hill - February 22, 2020