Subscribe

Latest Blog Post

part presentation playbook

Check This Out: 40 Universal Robots in One Room!

David Maltais
by David Maltais on Sep 10, 2017 2:47:02 PM

This is it. The Robotiq team is getting ready to Rock the #RUC2017!

Have you ever thought about installing 40 Universal Robots UR5 in one room? Well, this is exactly what we did today at the Bonne Entente Hotel, home of the Robotiq User Conference.

An army of 40 people from Robotiq, Universal Robots, Vention  and Sonoptik helped build this impressive setup, which will be used during the second day of the RUC to allow our partners and invited end-users to put what they've learned on day one to the test.

Here's a recap of a busy but funny day making the RUC come to life!

1-429126520899.jpgAn empty ball room awaits us in the morning

2-638.jpgEveryone is on task, building tables for a few hours

3.1.jpgThose tables are so much fun to assemble!

3.2.jpg
Life is always better when you smile

4-3.jpg
Tables are assembled, UR5 are getting installed

8.jpg
Our friends from Universal Robots flew from Denmark and the USA!

6.jpg

This is getting real...!

7.jpg

No time to spare, we're building the biggest cobots setup ever

9.jpg
Bonne Entente Hotel staff can't wait for the RUC to begin!

IMG_0687-1.jpg
We're all set! Stay tuned to see this factory in action during the #RUC2017

Subscribe to Robotiq's Blog and follow the RUC!

 
x

Subscribe to Robotiq's Blog

Leave a comment

David Maltais
Written by David Maltais
After a few years working as a journalist, David switched to corporate communications and public relations. He focuses on spreading Robotiq's voice around the world via medias, partners and influencers of the automation and manufacturing industries.
Connect with the writer:

Related posts

Who Talked About the RUC

Believe it or not, it's already been one week since the RUC ended. Our event photographer Frédéric Nadeau did some filming when...

David Maltais
By David Maltais - September 20, 2017
RUC 2017: The Wrap Up

 

-Inspiring Speakers -Launching The Era of Lean Robotics -Design, Integrate, Operate -24-Hour Workshop Challenge -Social...

Emmet Cole
By Emmet Cole - September 15, 2017
A Tribute to the RUC Participants

The 2017 Robotiq User Conference ended 2 days ago. I am still overwhelmed by the level of passion, competitiveness and...

Samuel Bouchard
By Samuel Bouchard - September 15, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more