Subscribe

Latest Blog Post

part presentation playbook

The Robots that Proctor & Gamble Dream About

Samuel Bouchard
by Samuel Bouchard on Jan 28, 2011 10:39:00 AM

 

Proctor gamble robotics resized 600

[Slide from P&G presentation at 2011 Robotics Industry Forum]

I had the chance to attend the 2011 Robotics Industry Forum event last week in Orlando, FL. One of the most interesting presentation was done by Mark Lewandowski, Machine Controls Technology Leader at Proctor & Gamble. The presentation created a unique setting whereby this extremely large company was telling an entire industry: "Guys, I am very willing to buy robots from you now, but you don't have what it takes!"

This point illustrates what I was discussing in a previous post : that current robots are not yet suitable for a very high number of potential end users. While I had mentionned this fact for SMEs previously, Lewandowski's presentation made me realize that this is also the case for massive non-automotive companies like P&G. And, this category represents an important market, considering that the robot density in packaging (Number of robots / employees) is less than 10% of what it is in the automotive sector (Source: World Robotics 2010).

Here are the specs of the ideal robot from P&G's point of view:

  • Smaller footprint and larger workspace
  • Lower integration cost
    • Use a modular "lego" approach to build systems out of standard building blocks.
    • Simplify the setup with basic functions already built-in
    • Have robots easily talk to other automation components such as PLCs.
  • Lower buying cost He said that a 50% lower cost could justify the ROI for a lot of applications.
  • Collaborative They spend a lot of money on guards to protect humans from robots. This also uses space where no value-adding process can be done. They'd like robots that are aware of their environment and the humans that surround them.

When I asked what features from traditional robots could be left aside, the only aspect he mentioned was their ruggedness. He stated, "You don't need massive casted parts in packaging." Still, he added, he would not want to compromise on speed, relability or precision.

Hubspot Material Handling Video Button

 
x

Subscribe to Robotiq's Blog

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel Bouchard is President of Robotiq, a fast growing robotics company based out of Quebec City, Canada, that he co-founded in 2008. He holds a Ph.D. in Mechanical Engineering and a bachelor in Engineering Physics from Laval University. He is also a regular speaker at international events on robotics technology and business.
Connect with the writer:

Related posts

Top 7 Robotic Applications in Food Packaging

Cakes, creams, lettuce and milk. Robots can package them all! Here are seven great robotic food packaging applications.

...

Alex Owen-Hill
By Alex Owen-Hill - August 16, 2017
What's New in Robotics This Week - Apr 21

Industrial & cobot roundup, meet the cheetah bot, drone brief (land & air), a good time to mention ISO/TS 15066, and much more. 

Emmet Cole
By Emmet Cole - April 21, 2017
What's New in Robotics This Week - Apr 14

Spot Bot joins the US Marines, manufacturing and cobot brief, new 3D computer vision challenge, TATA launches line of...

Emmet Cole
By Emmet Cole - April 14, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more