Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Classification of Robotic Grippers and the Next Generation

Samuel Bouchard
by Samuel Bouchard. Last updated on May 05, 2016 5:14 PM
Posted on Jan 14, 2014 8:29 AM. 2 min read time

 
In the world of robotics, both the industry and application environment determine the specific tool used at the end of a robot arm. This tool varies in definition from an EOAT (end-of-arm-tooling) to a manipulator or gripper. As automation applications become more complex and robots continue to be utilized for efficiency, the need for more versatile, dexterous grippers has emerged. Traditional grippers have features or classification criteria that are commonly given to them.

Classification Criteria of Traditional Grippers  

  • Types of Motion
    • Angular
      With angular grippers, the fingers close toward each other by rotating around an axis.
    • Parallel
      With parallel grippers, the fingers will approach each other remaining parallel.
  • Number of Fingers
    The vast majority of traditional grippers have two “fingers”. In fact, most of these fingers are not articulated. Other grippers can have 3 or 4 concentric fingers
  • Actuation
    Depending on application requirements, the gripper can be actuated by electric motors, pneumatic or hydraulic valves.
  • Size
    As there are a wide variety of sizes for robots, there is an equivalent variety of gripper sizes.
  • Pinch Force
    Because traditional grippers rely on friction to hold parts, pinch force is an important feature.

Next Generation of Grippers

A new generation of grippers have entered the market. These dexterous grippers are a unique convergence between grippers and hands. They typically have articulated fingers that can adapt to the shape of different objects. One example of such a gripper is the Robotiq Adaptive Gripper.

3-Finger-robot-gripper-end-effector-compliance-250px           3-grippers

These dexterous grippers will not replace all conventional grippers, they find their strongest use in applications where several traditional grippers would have to be used in conjunction with a tool changer to be able to properly grasp many different parts. The ability to use one tool for several applications (parts handling, parts transfer and sorting, picking and placing, kitting, etc.), or in the same work cell for a range of parts, greatly reduces tool changing time and setup costs.

Download this Free Guide on  How to Choose your Gripper Now

 

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

What's New In Robotics?  07.12.2018

-UR celebrates 10 years since 1st sale-China robot production data -World's first automated ferry -Hello Bennu-Elowan the...

Emmet Cole
By Emmet Cole - December 7, 2018
Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016