Subscribe

Latest Blog Post

compare new collaborative robots

5 Jobs Robots Can Do That Humans Don’t Want

Karen Smock
by Karen Smock on Aug 23, 2017 7:00:00 AM

Headlines about robots taking jobs are everywhere, but what exactly are those jobs, and do humans even want them?

Entering Unsafe Radiation Areas

The need for a non-human to enter dangerous radiation areas became a high priority after the damage to the Fukushima nuclear plant in 2011. Sciencemag reports that the maximum radiation levels discovered would have exceeded a human worker’s full year safety limits after exposure for less than one day. Military-grade robots had to be deployed to venture inside. 

In the following years, development of robots to step over debris and access damaged, contaminated areas has increased. A Wall Street Journal video shows HUBO robot creator Professor Jun-Ho Oh explaining that they created the robot to deal with a radiation contaminated area. 

automated-digging-and-loading-mining-robots-mining-automation.jpg


Hazardous Mining Jobs

The Mine Safety and Health Administration has tracked 76,000 deaths due to black lung disease since 1968. Breathing coal dust or risking being trapped in a collapse, cave-in, or a flooded mine is not a desirable job for a human.  Robots are welcome in mining to reduce hazards and to aid rescue operations

To be fair, not all mining jobs are so hazardous, and some less-hazardous jobs are also being automated.  As reported by MIT Technology Review, mining companies are taking advantage of automation to haul iron ore and drill. Just like other industries, automation eliminates some jobs while creating others such as maintaining the new equipment.

Low Wage Farm Work

US News reports that the specialty crop farm industry wants investments in mechanization and technology to offset labor shortages. Leaving the political debate about immigrant workers aside, what makes farm jobs unattractive? The New York Times cited a Georgia experiment using parolees to work farms that resulted in parolees quitting due to “intolerable working conditions.” The Bloomsburg Businessweek article Why Americans Won’t Do Dirty Jobs presented low wages, and back-breaking physical demands as reasons why the unemployed don’t want to pick produce, along with an attitude against doing farm work.

Picking soft fruits has been a challenge for robots, but new robotic strawberry pickers are already in field testing.  

Japan_Robot_Farm.jpg

Deburring and Other Repetitive Actions

Deburring is an excellent example of a repetitive, time-consuming, fatigue-inducing process prone to human error.  While flat parts are relatively easy to deburr using automation, curved pieces typically required traditional manual deburring. With robot end effectors becoming more sophisticated, they can adjust force to deburr rounded surfaces

Dull Retail Tasks

What’s worse than searching for someone to help you find something in a retail store? Being the person on the floor who constantly has to answer the same questions over and over. With autonomous retail service robots, customers can “ask” the robot, receive a reply in their choice of languages, and even follow the robot to the location of the item in the store. Lowe’s is using the LoweBot in select stores, and reports that the robots allow employees more time to offer specialty knowledge and expertise.  By leaving the routine searches and repeated questions to robots, human workers have higher job satisfaction.

lowe-bot.png

Transition Time

Automation is not going to go away, and jobs with a shortage of available or willing workers will be prime targets for robotic solutions.  Ideally, people will benefit from safer, more interesting work. But, as with most technology changes, the transition will likely not be easy for everyone to accept.

choose the right collaborative robot

 
x

Subscribe to Robotiq's Blog

Leave a comment

Karen Smock
Written by Karen Smock
Karen Smock is a freelance marketing and technical writer who specializes in manufacturing, manufacturing technology, and clear writing. She lives in a house where robots outnumber people.
Connect with the writer:

Related posts

What's the Difference Between Robotics and Artificial Intelligence?

Is robotics part of AI? Is AI part of robotics? What is the difference between the two terms? We answer this fundamental...

Alex Owen-Hill
By Alex Owen-Hill - July 19, 2017
What's the Difference Between Automation and Robotics?

Industrial automation, Robotic Process Automation, test automation… What do the terms all mean!? Are robotics and automation...

Alex Owen-Hill
By Alex Owen-Hill - June 28, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more