Subscribe

Latest Blog Post

get help with your robotic project

3 Types of Jobs People Hate That Robots Can Perform

Mariane Davids
by Mariane Davids on Aug 9, 2017 7:00:00 AM

The rise of robots has not taken our jobs, it has made them better. For people who work in manufacturing, there are plenty of tasks that can create long-term injuries or just take all the fun out of work. Whether they’re repetitive, hazardous, or just plain difficult, robots are here to make things easier.


3 Jobs Humans Hate That Robots Can Do

In the field of manufacturing, there are plenty of jobs that fall into categories people aren’t a fan of doing. Let’s take a look at three examples of work that robots don’t mind doing, but people can’t stand.

2F85-Wrist-camera-FT300-UR-Pick&Place-Box(1)JPG-439325-edited.jpg

1. Repetitive Assembly Work

It’s difficult to imagine working on an assembly line, but at the very least, it’s a repetitive process. You do the same thing, over and over, relentlessly for hours each day. Furthermore, if you get tired and you mess something up, it stop the entire process from working properly.

As time goes on, people who do this kind of work find themselves with debilitating conditions like carpal tunnel, or worse. It’s simply not the kind of work anyone wants to do. Companies like Foxconn have been dealing with employees becoming depressed and the issue is getting worse by the day.

That’s why companies like them have begun automating repetitive tasks in their manufacturing plants. These free up humans do more important and interesting things. Inspecting final products, handling precise assembly, things like this are more in line with human capabilities than robot ones.

2. Hazardous Work

Hazardous work is something humans don’t want to do, not because it’s boring, but because it’s downright dangerous! Robots don’t have to worry about situations like this, which is why it’s preferable that they handle these things.

Consider things like welding and sanding in manufacturing plants. The welding is self-explanatory, but the sanding could release particles into the air that aren’t good for people to be breathing.

Other tasks, like cleaning air ducts, can be done by smaller robots that fit into the tight spaces needed to complete such tasks. All of these represent potential dangers for humans, but rarely threaten robots.

3. Heavy Lifting

Robots began their lives in manufacturing as fenced cells that handled assembly of things like cars and other major industrial assembly lines. We’ve since been able to create collaborative robots that can work alongside humans. Whether it’s fenced robots assembling several-ton automobiles, or industrial tools, robots can handle it.

With the ability to assemble and move heavy objects, humans can avoid physical injuries or accidents. Amazon has been embracing this, with robots in their warehouses that move product around quickly, saving humans a huge amount of time and negating miles of walking each day.
choose the right collaborative robot

Final Thoughts

Humans have jobs they don’t want to perform, it’s just a simple fact of life. Why not give these jobs to robots and free ourselves up for more rewarding work? As this continues to happen, people are seeing the benefits of our automated coworkers. Which jobs are you glad robots are willing to do? Let us know in the comments!

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mariane Davids
Written by Mariane Davids
Mariane Davids is a social media marketer with over a decade of experience in the industry. She's now bringing her decade of experience to others so they can better connect with their communities.
Connect with the writer:

Related posts

What's New in Robotics This Week - Sep 08

 - Manufacturing & cobot roundup- John Deere acquires Blue River Technologies- Meet Musio - India's Ganpati bot and much more....

Emmet Cole
By Emmet Cole - September 8, 2017
How Procter and Gamble Is Leading the Way With Cobots

The consumer goods industry is starting to accept collaborative robots. Procter and Gamble is leading the way, and has been for...

Alex Owen-Hill
By Alex Owen-Hill - September 6, 2017
What's New in Robotics This Week - Aug 18

Manufacturing & cobot roundup, super self-healing soft bots, time to replace pets with bots?, A.I. set to reshape music and...

Emmet Cole
By Emmet Cole - August 18, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more